Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
FS7 IGBT Power TO247 3-Lead vs. 4-Lead

A comparison of the switching losses between the standard 3-lead and 4-lead TP247 devices can be seen here. The 4-lead device featured in this graph is a 140 A rated device. Comparing to the bar chart of the 3-lead devices to the left, the customer can see that the 140 A rated 4-lead device has much lower switching losses than even the 100 A, 3-lead S-series device. As mentioned before, this enables higher switching frequencies in power converters to help further reduce the size of magnetics in the design.

PTM פורסם ב: