Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
imrpoving color
In packages with multiple dies, spacing between the die is an important factor. ROHM’s manufacturing capabilities allow for a tighter internal 0.3 mm die spacing. When the distance between the die becomes smaller, there is an improvement in color mixture. As seen on the right, ROHM’s PICOLED-RGB tighter die spacing provides the benefit of wider and richer color mixture.
PTM פורסם ב:
PTM Updated on: 2018-08-27