Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
MK31 Series 1

The latest edition to Standex Electronic’s line of SMD reed sensors is the MK31 Series. Featuring a powerful, robust and miniature design that is 20% smaller than the competition (measuring only 6.4 mm x 1.95 mm x 2.2 mm), the MK31 Series can switch a minimum of 50 million reliable operations in a wide variety of low-power and space-limited applications. Although slightly larger than the MK24 series, the MK31 SMD reed sensor differs from the MK24 series in that its contact gap is in the center of the sensor which allows the actuator magnet to be placed directly over the gap position for optimized sensor function. Also MK31 has a longer lead on one side of the sensor giving it a larger sensing distance than the MK24 series.

PTM פורסם ב: