Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
AC Switches Family - Part 2 Slide 7

There are many different types of packages, from the least expensive TO92, through the various standard packages that are well known today, and in the isolated packages, the insulated TO220 and the insulated molded plastic fullpack package. Also shown is the isotop which is used for very high-current applications, not a very common part, mainly found in welding applications.

PTM פורסם ב: