Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
cSPIN Slide 13
Another important feature offered by cSPIN is the digital diagnostics. A full set of diagnostic information can be read through the SPI interface, such as thermal warning and thermal shutdown, undervoltage lock out, overcurrent protection or stall detection, and this can be easily queried from the internal register, without the need for further external circuitry.
PTM פורסם ב: