Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
cSPIN Slide 4

The new cSPIN family offers two devices: the L6480 and L6482. The L6480 uses a novel technique based on voltage mode to reach high performances and the finest smoothness. The L6482 uses a current-control technique, enhanced by an ST patented predictive algorithm. They both have a logic core to fully manage the motion and an SPI to communicate with the application microcontroller.

PTM פורסם ב: