Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Digital MEMS Microphones Slide 20

The frequency response curve for ST’s MP34DT01 top-port digital MEMS microphone is shown on this slide. As can be seen, the response of the MP34DT01 is only down about 1dB at 20Hz and about 0.5dB at 20KHz, and is absolutely flat between 100Hz and 10KHz.

PTM פורסם ב: