Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Digital MEMS Microphones Slide 23

Shown on this slide is the x-ray of ST’s MP34DT01 microphone that was shown on a previous slide. It is possible to clearly see the metal shielding that exists inside the microphone. The IC and the sensor itself are completely shielded from the external world by an internal Faraday cage, which provides good EMI performance.

PTM פורסם ב: