Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
iNemo Slide 13

The image on this slide depicts the operation of Sensor Fusion. The Sensor Fusion is located with the hardware and drivers. The kernel of the system and the sensor fusion algorithm will be running to feed the end user application. The end user application will call the functions from the header files to get the compass or whatever tracking is desired.

PTM פורסם ב: