Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
iNemo Slide 4

At the present time there are four available solutions, as shown on this slide. The first is the iNEMO Engine LITE, which is a light version and will help to the user understand how it all works. It is available in source code. The other three versions, are grouped within a common category called the PRO version, or more specifically the iNEMO Engine PRO. There are three versions of iNEMO Pro; first is the Android platform, the second is platform independent, STM32- or other micro MCU-based, with no special OS, and the last is the Windows 8 version. In essence there are two categories, the LITE version, available in source code and the PRO, which is higher in performance. The PRO version is not available in source code, it is pre-compiled.

PTM פורסם ב: