Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
acepack main tops

The beauty of a power module is that designers are not limited to only one electrical topology (as they are with an IPM). A power module can be used to drive an electric motor (as a 3-phase inverter) or can be used for a generic power conversion stage (an n-phase interleaved PFC stage). Very complex topologies, like multi-level inverters, can be realized with a power module drastically improving the compactness of the board while reducing the parasitic elements that become more and more relevant as the power increases.

PTM פורסם ב: