Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 37

If the transfer function that was derived in the discussion on minimum current is applied to the desired sine wave current for microstepping, the effect of minimum current shown here in the orange and green occurs. If the output of the DAC sets current near zero, the circuit will respond with the minimum current. To get zero current, the bridge can be disabled and all of the transistors can be turned off. Without any drive, the current will go to zero in order to get the zero points on the sine wave. Since zero current is possible, look only at what affect the minimum current will have on the sine wave just before and just after the zero value. Luckily the first micro step after zero and the last one before zero is the largest step that is needed. So if the minimum current is less than the sine of the first microstep, there should be no distortion in the sine wave. In the example shown here, the minimum current starts to effect the waveform at about 11°. So if the first microstep is more than 11°, there should be no distortion on the sine caused by the minimum current. In this case, each quarter cycle could be divided into eight microsteps of 11.25° each.

PTM פורסם ב: