Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 9

The answer is that there are actually some states halfway between the full step positions that the motor can easily be driven to. These positions are obtained by simply turning off the current in one coil before turning it on in the opposite direction. Here, state 1, 3, 5, and 7 are the same as the full step sequence shown before. States 2, 4, 6, and 8 have current in one winding and no current in the other. Since these positions are halfway between the full step positions, they are referred to as half steps. The drive sequence to operate the motor in half step then has 8 states per electrical cycle. The advantage is that the number of steps per revolution can easily be double, so a 1.8° per step motor now gives 0.9° of resolution.

PTM פורסם ב: