Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
LED Lighting Driver Solutions Slide 9
By reducing the size of the input capacitor required and applying an inductor current regulating scheme, in-rush current is managed to be less than 1.5 A using the TI TPS92560. By limiting the amount of in-rush current drawn from the electronic transformer, not only the life time of the transformer is improved, but also the possibility of an electronic transformer driving several MR-16 LED bulbs in parallel instead of an usual 1:1 (one electronic transformer to one MR-16 bulb) driving limitation.
PTM פורסם ב: