Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Topic 8 ControlSUITE Slide 11

Those familiar with the C2000 device previously will be completely at home writing software for the Control subsystem. Almost everything in ControlSUITE for the Control Sub-system is the same as with previous devices. For instance, register access is identical to a Piccolo device using that structure register access mechanism. Special function libraries and peripheral drivers are also largely the same, with a few exceptions. There is also the Viterbi, Complex Math, and CRC Unit, which will be covered on the next slide.

PTM פורסם ב: