Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Topic 8 ControlSUITE Slide 20

TI is also providing several host mode examples. Once again, a keyboard and mouse examples, but instead of emulating a keyboard or mouse, this time, one can plug a keyboard or mouse directly into a Concerto device and read either key presses or mouse movements and button presses from those devices. TI is also providing a host to mass storage class example where one can connect a thumb drive directly to a Concerto device and read and write the file system present on that device. Then a flash boot loader that can load firmware via a USB thumb drive to be released.

PTM פורסם ב: