Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
eZ430 Development Tool Overview Slide 18

By default on a Windows installation, the Chronos software will download to C:\Program Files\Texas Instruments\eZ430-Chronos. There is also a package available for Linux. Included in this software package is the Control Center, which is the program that interfaces with the watch, the data logger and the binaries are both included which means the program that opens and the source code for both of those applications is available. The documentation provided in the download include the Chronos user guide as well as schematics, Gerber files and BOMs for the RF Access Point, eZ430 debug interface and watch. Additionally, this download includes the RF Access point Driver, Binary images and multiple software projects.

PTM פורסם ב: