Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
eZ430 Development Tool Overview Slide 8

The other protocol on the Chronos is from a company called BM Wireless and the stack is called BlueRobin™. BlueRobin™ is compatible with a couple of heart rate monitors and some biking equipment, such as speedometers. It supports long range monitoring systems for body area networks like pedometers and heart rates. BlueRobin™ also supports bi-directional data which is encrypted for security. Since it has the library built in, if the user follows the BlueRobin™ API, they should be able to communicate with external devices. The one negative of BlueRobin™ is that it is not an open-source protocol stack, it is only provided as a library. For specific BlueRobin™ questions the designer will have to go directly to BM Wireless for support.

PTM פורסם ב: