Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Thermistor and RTD Probes and Assemblies Slide 3
The first step in designing or selecting a temperature probe assembly is to determine the environment (operating and non-operating) into which the probe will be subjected, as well as any significant mechanical or thermal stresses to which the sensor may be exposed during the installation or in the assemblies use. Environmental factors include the application's temperature range, thermal cycling and/or thermal shock, chemical exposure, humidity as well as mechanical stresses.
PTM פורסם ב: