Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Thermistor Resistor Network Simulation Tool Slide 12

Re-running the computation with changes to the input voltage variation will affect the output. In the output shown here, the voltage variation was input at 5 mV/°C which is much lower than the 25 mV/°C input in the preceding run. The voltage variation change resulted in the computation choosing a linear PTC as the best fit instead of an NTC. It can also be noted that one of the fixed resistors is non-existent in this case. That’s because the tool provides the fixed resistors only when necessary.

PTM פורסם ב: