Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Thermistor Resistor Network Simulation Tool Slide 8

The TNPW series is available in tolerances up to ±1%, however the tool only allows selection of the highest precision tolerances. The high precision tolerances assist in achieving the most accurate network solution possible. As the fixed resistors present a variation with temperature, although much less than the thermistor, the program will still take account of this temperature coefficient of resistance. If the fixed resistors are remote from the thermistor, the temperature variation seen by the thermistor is not applicable to these fixed resistors. In this case, select option “0” for the TCR.

PTM פורסם ב: