Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
VY Series Slide 3

There are two types of Radio Frequency interference that X and Y capacitors address. The first type is broad band interference that is generated by power lines, electric motors and  switching. The second type is narrow band interference and is the result of signals that are intentionally generated from sources such as cell phones, radio transmitters, and other communication devices. Regardless of the source of the interference, it can be propogated via wire conductors, radiation or capacitive and inductive coupling.

PTM פורסם ב:
PTM Updated on: 2015-09-08