Thermal interface materials are what makes sure that the thermal transfer between the heat source and the cooling assembly is as efficient as possible. Even though the contact surfaces of the heat source and the cooling assembly seem flat and coplanar, microscopic irregularities have a huge toll on the thermal performance of the system. Thermal interface materials make sure that there are no gaps between the heat source and the cooling assembly and provide a low thermal resistance path for heat to flow through.