Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Image of Würth Elektronik Thermal Interface Materials - TIM Continued

These materials can be divided in two groups: gap fillers and heat spreaders. Gap fillers are great to provide an interface between a source and a cooler, while heat spreaders transport heat in a horizontal plane to distribute it along a surface. The bigger the surface spread, the more energy transfer to the ambient. This is particularly relevant when working with enclosures.

PTM פורסם ב: