Maker.io main logo

OOZE MASTER 3000: NeoPixel Simulated Liquid Physics

134

2025-05-30 | By Adafruit Industries

License: See Original Project LED Strips Adafruit Feather

Courtesy of Adafruit

Guide by Phillip Burgess

Overview

led_pixels_oozemaster-thumb

This project lets you dress up a window, Halloween prop or wall decoration with eye-‎catching LEDs that simulate dripping liquid but leave no mess behind…it’s a completely dry ‎effect!

Also, just changing the color and the prop, this is perfectly usable for Christmas decor as ‎well. This is one of those “sandbox projects” that can fit wherever your imagination takes ‎it…I’m just really partial to Halloween, so that’s what’s demonstrated here. Raawr!‎

The idea for this stemmed from three things…‎

First: the arrival of some incredibly skinny NeoPixel strips…just 4mm wide! From any ‎reasonable viewing distance, they almost disappear. As explained on the next page, bigger ‎projects may do just fine with regular-size NeoPixel strip, easier to work with.‎

Second: our NeoPXL8 FeatherWing and NeoPXL8 Friend boards are designed to run up to 8 ‎NeoPixel strips concurrently. Most folks focus on the speed of this, but I’d been looking for ‎a project to showcase the topological benefit…that each strand doesn’t need a return line ‎to the next. We use this to make “drips” that end in mid-air.‎

strips_1

strips_2

Third: I’m a sucker for any project using age-old theatrical tricks with new technology…the ‎simplest thing is suddenly indistinguishable from magic…‎

Each of our “drips” briefly makes a “splat” where it lands…but there’s an air gap there, not a ‎contiguous strip of NeoPixels from top to ground. It’s like a one-pixel version of a film ‎editor’s cutting on action: hero throws knife, cut to villain with knife in his chest. Timed just ‎right, we see a continuous motion out of two separate shots. Similarly, our dot jumps ‎from A to B just when you’d expect, and the brain fills in the story. Brains are hilarious.‎

Things You’ll Need

Read through the whole guide before making any purchases…it’s full of tips and ‎alternatives, and your build will probably end up slightly different. Additionally, skim ‎the NeoPXL8 guide for the latest on compatible hardware…several M0, M4, RP2040 and ‎ESP32-S3 Feather boards can now work with this, though each may require some ‎tweaks. But in general, you’ll need these items:‎

  • A NeoPXL8-compatible development board such as the Feather M0 Basic ‎Proto, Feather M4 Express, Feather RP2040 or Feather ESP32-S3, and ‎some headers. Some non-Feather boards can work as well, but connections are ‎usually simpler with this form-factor. Please see the NeoPXL8 guide mentioned ‎above.

  • NeoPXL8 FeatherWing or NeoPXL8 Friend. There are two distinct versions of the ‎FeatherWing: one intended for M0 Feathers, one for M4. The two are ‎generally not interchangeable, with an exception for the easy-going Feather ‎ESP32-S3 that can use either. The “Friend” is a breakout version for non-Feather ‎boards.

  • Or…the Feather RP2040 SCORPIO combines microcontroller and NeoPXL8 into ‎a single board!

  • NeoPixel strips and pixels (explained further in guide)‎

  • Lots of wire

  • Soldering iron and related paraphernalia

  • Sundry craft supplies and tools; this will vary with how you decide to implement the ‎project. There will almost certainly be hot glue involved…but I also found myself ‎using masking tape, a permanent marker, hobby knife, foam core board and acrylic ‎paint.‎

Planning

I picked up this plastic dragon skull candy dish among the seasonal merchandise at a ‎local big-box store. Mostly because I like dragons. But also…tell you a secret…I wasn’t ‎certain this idea would work. The dragon skull was a good size for a Monster M4sk eyes ‎project as a Plan B!‎

planning_3

In hindsight, I’d recommend aiming bigger. Lots of stores have hanging ghouls, werewolf ‎skeletons, elaborate foam tombstones and so forth, any of which would look fantastic with ‎some ooze!‎

Reason I suggest this is because big props are more to-scale with classic NeoPixel strip, ‎which is easier to work with. The ultra-skinny strip is amazing but ‎requires patience and top-level soldering skill.

I already had the dragon skull though, so that’s what I’ll walk through here…‎

planning_4

Photo credit: Target

Oozes and Dribbles and Drips, Oh My!‎

The ooze (or blood, or water) animation along each NeoPixel strip follows a certain ‎sequence…‎

  • An initial “oozing” from a single point…like a tear will well up in your eye before ‎falling.‎

  • A slow “dribbling” part way down the strip…think of the tear now trickling down your ‎face to your chin.‎

  • “Dripping,” falling from chin to ground.‎

  • A “splat” where it hits the ground.‎

These distances are all configurable in the software on a per-strip basis. The way that ‎everything oozes, dribbles and drips along different lengths gives it a more natural (or ‎supernatural?) appearance.‎

The dribble portion requires a contiguous length of NeoPixel strip. The drip only needs to ‎cover about half the distance to the splat…it just ends in empty air, and the single ground ‎splat NeoPixel completes the illusion.‎

Measure and Plan

Look over your Halloween prop and decide where your dribbles and drips will go, and ‎measure distances to figure how many NeoPixels you’ll need. Remember that you’ll need ‎to span the full distance of a dribble, and about half the distance of a drip.‎

NeoPixel strips come in specific densities and lengths. If your total works out to just a few ‎pixels over such a threshold, it’s OK to shorten some drips by a pixel or two…the illusion still ‎works.‎

I found that this dragon had a slight underbite, and drips from the nose would have landed ‎on the lower teeth. While that’s possible and would look cool, I wanted to keep it simple with ‎all the drips on the table. Scrounging in the garage for any piece of junk, I found this spray ‎can cap and hot-glued it at the rear base of the skull to tip it forward a bit, problem solved.‎

Splat positions and numbers (0 to 6, corresponding to each drip) are marked on the ‎base…these distances are needed later.‎

Base was a piece of foam core board, but just about anything the right size would work…a ‎piece of wood, cardboard box flap, or a plastic serving tray.‎

measure_5

measure_6

measure_7

NeoPXL8 Topology

The code and hardware for the OOZE MASTER 3000 can animate up to 7 “drips,” with ‎an 8th wire driving the “splats” on the ground. Here’s a schematic view showing the ‎NeoPXL8 FeatherWing and NeoPixel strips:‎

schematic_8

THINGS TO KNOW:‎

  • This is a schematic diagram, not a literal wiring diagram. Look closely at your ‎NeoPixel strips, they often have input pads in a different order.‎

  • You can have fewer than 7 drips if you want but always start from NeoPXL8 ‎output #0. The splats are always on NeoPXL8 output #7.‎

  • Your drips will probably a mix of lengths!‎

  • The Feather RP2040 SCORPIO board came along later, but the principle is exactly ‎the same…connections are simply at one end of the board rather than down the ‎middle.‎

Q: What if I want more than 7 drips?‎

A: Some options…‎

  • You can drive 8 drips from one board, but you won’t get ground splats in that case.‎

  • You can just build multiple units. There’s nothing that needs to be synchronized ‎between them.‎

  • It’s possible to split the output signals if you’re OK with duplicate identical drips in ‎places…this is discussed on the last page.‎

Ground “Splat” NeoPixels

For the “splat” NeoPixels, where each drip hits the ground, I used several of these “Mini ‎Button PCB NeoPixels,” one per drip — but there are lots of other options, depending on ‎soldering skill and available resources…‎

Flora RGB Smart Pixels and Breadboard-friendly RGB Smart NeoPixels can also be ‎individually soldered into a chain. Or, if the pixel spacing works for your project, this ‎NeoPixel LED Strand might avoid a lot of intricate soldering.‎

If you’ve done projects with NeoPixel strip previously, or if that’s what you’re using for your ‎‎“drips,” odds are you have a few strip end-trimmings that you’ve held onto. These can be cut ‎to individual pixel strandlets and then solder wires between them.‎

ground_9

Power

I decided to power my dragon from the Feather board’s USB port, plugged into either a USB ‎charger or power bank. This just made everything a lot easier…using a bare LiPo battery ‎would require a couple extra components and expense, but everyone has a spare charger ‎and USB cable.‎

To distribute power to all the LED strands, I sawed some of the power rails off a Perma ‎Proto PCB and soldered this to the NeoPXL8 FeatherWing’s USB (5V) and GND pins with 22-gauge wire.‎

There are other ways this could be done, but being able to “home run” all of the power to this ‎one spot made things easier to keep track of.‎

power_10

power_11

Wire

You are going to need SO. MUCH. WIRE. Even just this little dragon centerpiece, about 13 ‎inches long, used about 30 feet of wire, divided evenly between red, black, and green (to ‎better keep track of 5V, ground and data wires).‎

For the dragon, I used 26-gauge stranded wire throughout (except for the two thicker wires ‎to the power distribution rails). Even 28 gauge would suffice, as it’s a tiny project. For ‎something bigger…more pixels or longer distances…consider using heavier gauge wire for ‎power and ground but keep the data wires thin.‎

If your project is something like the hanging ghoul (or simply dressing up a window frame), ‎with some distance between the “drips” above and “splats” below, it should be fine running ‎wires a few feet to the splat NeoPixels. There’s no defined hard limit I can provide, ‎sometimes you just have to build and adapt…I’d feel confident running wires 4 or 5 feet, but ‎‎10 feet or more just seems iffy for the signal to get through reliably.‎

Base

You’ll want each “splat” aligned with the “drips” from above…meaning they’ll need to be ‎glued, taped or zip-tied in place.‎

For the dragon centerpiece, I used a piece of foam-core board and hot-glued each pixel in ‎place (after all the wiring was done…more of that is explained on the next page).‎

Build Part 1‎

Here I’ll show some of the steps that went into my dragon. You’re probably building ‎something different, so don’t consider any of this to be canon law, just some ‎helpful tips and observations along the way…‎

I was super lucky with this dragon. Opening it up to see where electronics would fit inside, I ‎found that all the drips would come through this one skull piece.‎

You don’t have to conceal the electronics deep inside your project. Maybe they’ll fit behind. ‎Or if you’re decorating something like a skeleton, pick wire colors that conceal well (like ‎black or white) or can be passed off as part of the gag (e.g., red and blue wires as arteries ‎and veins).‎

build_12

Cutting NeoPixel strands.‎

LABEL EVERYTHING AS YOU GO. The drips are different lengths, so it’s important to keep ‎track of which drip is #0, #1 and so forth…‎

strands_13

Soldering to these Ultra Skinny NeoPixel strands is quite challenging. This is why I ‎recommend most folks make a bigger prop using “normal” NeoPixels.‎

The solder pads on these strips are really tiny (just a couple of millimeters after cutting) and ‎not clearly labeled (I cut the strips from the bottom and kept the original “head end” around ‎for reference). You can scrape away a little extra contact area with a hobby knife. Tin the ‎pads and the stripped wire ends with solder…‎

soldering_14

Even a “third hand” tool wasn’t much help with these connections. I just taped the strip ‎down right on my grungy workbench and held down each wire against the bench while ‎soldering, one-by-one.‎

Oh! Also worth mentioning: these strips have double-stick tape on the back, which is not ‎helpful for our drips. Working slowly, it’s possible to carefully peel this tape off the strip. ‎There might be a bit of lingering stickiness, but you can just paint over this later.‎

The splats are a lot more straightforward…tin the pads, tin the wires, solder them together. ‎It’s just a whole lot of wire.‎

Keep careful track of the order and distances between splats…#0 to #1 will be different ‎than #1 to #2, and so forth…it all depends on your drip placement.‎

Give yourself a little extra length between your splat pixels, so you can fine-tune their exact ‎placement later.‎

wires_15

All the drips and splats. So many pixels! So much wire!‎

This isn’t really part of the assembly instructions, I just worked really hard on this and ‎wanted to be sure everyone saw.‎

wires_16

MANDATORY TESTING

I cannot emphasize this enough: after soldering, you must test every single strand before ‎proceeding. This helps weed out any weak or wrong connections, bridged solder joints…or ‎occasionally the first pixel in a strand can be killed by heavy-handed soldering (if this ‎happens, clip it off and re-solder starting at the second pixel, it’ll look fine).‎

Load up the NeoPixel strandtest example…either on the Feather M0 board you’re using for ‎this project, or any other board you have around…change the code’s pin ‎number and strand length to match your longest strand.‎

NeoPixels should not be connected to a live circuit. Make the connections, then power up ‎the board.‎

Yes, this is tedious. But it is 1000% necessary. If you build the whole project and then find ‎something wrong buried deep inside and unreachable, you will cry.‎

testing_17

Build Part 2‎

Have you tested all of your NeoPixel strips at this point? Because I swear, I will turn this ‎car around.‎

Start placing your drips, securing them in place with hot glue, Krazy Glue®, zip ties or ‎whatever your install calls for. Some wires here simply fit through the eye or nose openings, ‎while others I drilled small holes through the skull.‎

The number labels were moved to the data wire for each strip. Must keep track of those!‎

Don’t worry if the strips hang outward at weird angles…just get them attached and ‎straighten them out afterward.‎

Also: DON’T BE LIKE ME. I glued down all the “splats” before the drips, based on my earlier ‎estimates of their positions. Much better to install the drips first, see where ‎things actually hang at that point, and then glue down the splats, fine-tuning their positions ‎as needed! Mine are a bit off.‎

part_18

part_19

You’ve been grappling and rough handling these NeoPixel strips…so, I’m sorry, but it’s ‎a really good idea to test them all again and fix any problems now, when they’re still ‎accessible.‎

part_20

Did you test everything again? Okay good…‎

Down the middle of the NeoPXL8 board is an 8x2 header. One row of this is the NeoPixel ‎data outputs, the others are grounds. For this project we’ll be soldering only to the ‎NeoPixel outputs (with the numbers just above them), not the ground points (with “–” ‎below). Plus of course the USB and GND wires mention earlier, to the power bus.‎

Starting to make connections from the first two NeoPixel strips to the NeoPXL8 FeatherWing ‎and my makeshift power bus.‎

As a sanity-preserving measure, I had simply soldered identical foot-long wires onto every ‎strip rather than measuring out each one ahead of time. Now at this stage I clip off a couple ‎inches, whatever’s actually needed to reach from point to point, with a little slack so I can ‎still move things around while working on this. Wastes a little wire but saves a lot of time.‎

Keen-eyed readers might spot there’s two data wires going to NeoPXL8 outputs #0 and #1. ‎Yours might not need that…it’s something covered on the Extra Drips page.‎

connections_21

Soldering wires directly from the top skull to the base was just asking for trouble…I knew ‎there would be a lot of wrestling parts into place here.‎

I added a 3-pin JST SH plug and receptacle so the two parts could be separated while ‎working on them. This turned out to be really helpful during assembly (I could plug that in ‎later as a next-to-last step), but also just in case I needed to go back inside for ‎maintenance. Strongly recommend this for your splat pixels!‎

plug_22

plug_23

All power and data wires connected, including the JST plug for the splat pixels.‎

An important step…not shown here…was to load up the NeoPXL8 strandtest example and ‎sort out the correct pinout for the board we’re using as explained in the NeoPXL8 ‎guide…sometimes the FeatherWing needs some traces cut and jumpered, and this is the ‎last time you’ll have easy access to the board.‎

With the basic NeoPXL8 test sorted out, oad up this project’s OozeMaster3000 Arduino ‎sketch, copy over the pin array you worked out for strandtest, and test it all again. Even if ‎not using the final settings, just making sure there’s no shorts or bad pixels. The code is ‎explained on the next page. Later we’ll make further tweaks for the actual strand lengths.‎

After it all checked out, I glopped up these wires with hot glue to provide some strain ‎relief when this gets stuffed into the skull and similarly covered the back side of the power ‎bus to prevent it shorting on other parts.‎

datawires_24

datawires_25

Since the Feather board will be buried inside this skull, I connected a micro-USB ‎cable and hot-glued it in place, so it won’t fall out, then fed the other end out an opening at ‎the back of the skull.‎

If you do this, make absolutely certain it’s a USB charge and sync cable, not a charge-only ‎cable! Please test this first. A charge-only cable can provide power but won’t let you update ‎the software on the board.‎

Wiring’s done, sealing up the skull. You can just make out the hot-glued USB cable here.‎

And yes, test it all again.‎

testagain_26

testagain_27

The NeoPixel strips running along the skull are pretty conspicuous, so I camouflaged them ‎with some cheap craft store acrylic paint.‎

Don’t sweat it if your painting is sloppy or colors don’t match. Five feet away, nobody will ‎notice.

If you get paint over any of the NeoPixels, it can be scraped away with a toothpick, or a Q-‎Tip® dipped in rubbing alcohol.‎

To conceal the wires inside the skull, I stuffed some wads of black chiffon that I found in my ‎crafting hoard.‎

paint_28

paint_29

paint_30

As a last step, I cut a circular skirt from thin fabric and placed this over the base. It hides the ‎‎“splat” electronics while still letting enough light through to complete the illusion…you can ‎see this in the project’s title image.‎

Arduino Code

The software for this project uses the Arduino development environment. If this is your first ‎time using this with Adafruit boards, please see the Feather M0 Setup guide here:‎

Adafruit Feather M0 Basic Proto: Arduino IDE Setup

Aside from installing the Arduino software, you’ll need to add the Adafruit boards ‎package as mentioned in the guide above.‎

Other boards…M4, RP2040, ESP32-S3…will have corresponding starter guides to get these ‎going with the Arduino IDE. If it’s your first time using them, use the search field to locate ‎those guides.‎

Additionally, you’ll need a few prerequisite libraries, which can be installed with the ‎Arduino Library Manager (Sketch→Include Library→Manage Libraries…). Search for and ‎install:‎

  • Adafruit_NeoPixel

  • Adafruit_NeoPXL8‎

  • Adafruit_ZeroDMA

Then fetch the code for this project, downloadable here:‎

Download OozeMaster3000 source code for Arduino

Select “Feather M0” (or whatever board you’re using) from the Tools→Board menu, compile ‎and verify that you can upload to the board. If so, great! Now we need to fine-tune some ‎settings to match your project…

If using a Feather M4 (with M4 version of the NeoPXL8 FeatherWing), look for this line early ‎in the code:‎

Download File

Copy Code
int8_t pins[8] = { PIN_SERIAL1_RX, PIN_SERIAL1_TX, MISO, 13, 5, SDA, A4, A3 };

Change the list of pins to the following:‎

Download File

Copy Code
int8_t pins[8] = { 13, 12, 11, 10, SCK, 5, 9, 6 };

The above change is only needed for Feather M4; if using Feather M0, you can leave the ‎defaults.‎

Other boards will use different pins. If you’ve worked through the NeoPXL8 guide and ‎puzzled through the strandtest example, this should all be sorted out by now. If using a ‎Feather RP2040 SCORPIO, the sketch takes care of this part.‎

Now we can configure some visual things…‎

Near the top of the code is this line:‎

Download File

Copy Code
#define PIXEL_PITCH (1.0 / 150.0) // 150 pixels/m

This tells the code the “density” of your NeoPixel strip, in LEDs-per-meter. The default, ‎‎150.0, corresponds to the density of the ultra-skinny NeoPixel strip. If using different pixels, ‎change this to match…60.0 and 144.0 are both pretty common strip densities. The code ‎needs to know this figure, so the drippings fall at a physically plausible speed.‎

Q: Can I mix and match strip densities?‎

A: Electronically there’s nothing preventing this, but the code as written works with a single ‎density throughout.‎

Speaking of physically plausible speed, look for this a few lines further down:‎

Download File

Copy Code
#define G_CONST 9.806 // Standard acceleration due to gravity

‎Combined with the strip density figure, this makes the drips fall convincingly. 9.806 is the ‎force of gravity on Earth, in m/s2. A little math ties this all together to make the drips and the ‎splats play well together and fool your brain.‎

The value there…9.086…is convincing enough for a thin liquid like water or blood. If you ‎want something really viscous looking…rather than working viscosity calculations into the ‎code, you can be like Q from Star Trek and just change the gravitational constant of the ‎universe. Try values between 2 and 3 for a nice gravy-like feel.‎

Then, a short way down, look for this section:‎

Download File

Copy Code
uint8_t palette[][3] = {
  { 0, 255, 0 }, // Bright green ectoplasm
};

This defines the color of the drippings, as an RGB value. The default, {0,255,0}, is a pure ‎green…good for ectoplasm. But you might want red instead, {255,0,0} for blood, or blue ‎‎{0,0,255} or white {255,255,255} for something more Christmasy. Later we’ll explain how ‎to use multiple colors.‎

One more piece to this recipe…a little further along in the code, look for this table of ‎numbers:‎

Download File

Copy Code
// THIS TABLE CONTAINS INFO FOR UP TO 8 NEOPIXEL DRIPS
  { 16,  7, 0.157, 0, 0 }, // NeoPXL8 output 0: 16 pixels long, drip pauses at index 7, 0.157 meters above ground, use palette colors 0-0
  { 19,  6, 0.174, 0, 0 }, // NeoPXL8 output 1: 19 pixels long, pause at index 6, 0.174 meters up
  { 18,  5, 0.195, 0, 0 }, // NeoPXL8 output 2: etc.
  { 17,  6, 0.16 , 0, 0 }, // NeoPXL8 output 3
  { 16,  1, 0.21 , 0, 0 }, // NeoPXL8 output 4
  { 16,  1, 0.21 , 0, 0 }, // NeoPXL8 output 5
  { 21, 10, 0.143, 0, 0 }, // NeoPXL8 output 6

The table holds information about our NeoPixel strips and real-world distances, to make ‎the physics “actual size.” Each line, one for each drip (up to 7) contains three numbers:‎

  1. ‎The length of the NeoPixel strip, in pixels.‎

  2. The pixel index (starting at 0, up to length-1) where the dribble pauses before ‎falling. This can be 0 if you want no dribble.‎

  3. The distance from the dribble pixel (the one you just provided the index # for) to the ‎splat pixel below, in meters.‎

  4. A range of color indices to use from the palette[] array. With just one color defined for ‎the default example case, both of these values are 0.‎

You can have an 8th drip but won’t get splats in that case. Given a choice, I think the splats ‎are way cooler.‎

Here I’m measuring drip-to-splat length for drip #6. It’s about 143 millimeters, or 0.143 ‎meters as you can see in the table. Not the topmost pixel, not the end of the drip, but ‎the dribble pixel at the tip of the horn.‎

If measuring in inches, multiply by 0.0254 to convert to meters.‎

measure_31

Get all your numbers and measurements in there, save the code (or a copy) and upload to ‎your Halloween prop. If all goes well, the motion should physically correspond to the thing ‎you’ve built! If it’s close but not quite, tweak your table numbers…move the dribble pixel up ‎or down a bit, change distances (or G_CONST) to get the timing right.‎

Colors and Effects

To avoid being too overwhelming, the default code has everything a single color by default. ‎We can amp this up, but it’s going to involve more numbers.

First, look again at the palette[] section of the code:‎

Download File

Copy Code
uint8_t palette[][3] = {
  { 0, 255, 0 }, // Bright green ectoplasm
};

This can be expanded to a list of colors. Each {in curly braces} is three numbers — red, ‎green and blue components, each in the range 0 to 255. Mind your commas and ‎formatting!‎

For a Fourth of July aesthetic, one might choose a palette like this:‎

Download File

Copy Code
uint8_t palette[][3] = {
  { 255,   0,   0 }, // Color 0 = Red
  { 255, 255, 255 }, // Color 1 = White
  {   0,   0, 255 }, // Color 2 = Blue
};

Next, we tell the drips[] table what colors to use, using indices into the palette[] array. ‎Because of the way C arrays work, this numbering starts at 0.‎

The last two numbers for each drip are the lowest and highest color palette indices to use. ‎A color within this range will be randomly picked each time a new drip starts there:‎

Download File

Copy Code
} drip[] = {
  { 16,  7, 0.157, 0, 2 }, // Randomly pick from palette 0-2
  { 19,  6, 0.174, 0, 2 },
  { 18,  5, 0.195, 0, 2 },
  { 17,  6, 0.16 , 0, 2 },
  { 16,  1, 0.21 , 0, 2 },
  { 16,  1, 0.21 , 0, 2 },
  { 21, 10, 0.143, 0, 2 },
};

‎Perhaps you just want each drip a distinct color, not randomized. NeoPixel rainbows are ‎popular…maybe a bit overdone, but some occasions do call for it. One sets up a color ‎palette:‎

Download File

Copy Code
uint8_t palette[][3] = {
  { 255,   0,   0 }, // 0 = Red
  { 255, 160,   0 }, // 1 = Orange
  { 255, 255,   0 }, // 2 = Yellow
  {   0, 255,   0 }, // 3 = Green
  {   0, 255, 255 }, // 4 = Cyan
  {   0,   0, 255 }, // 5 = Blue
  { 192,   0, 255 }, // 6 = Purple
};

‎…and then, in the drip[] array, both numbers at the end of each drip are set to ‎the same palette index:‎

Download File

Copy Code
} drip[] = {
  { 16,  7, 0.157, 0, 0 }, // Always use palette[0] for this drip
  { 19,  6, 0.174, 1, 1 }, // and palette[1] for this drip
  { 18,  5, 0.195, 2, 2 }, // and so forth...
  { 17,  6, 0.16 , 3, 3 },
  { 16,  1, 0.21 , 4, 4 },
  { 16,  1, 0.21 , 5, 5 },
  { 21, 10, 0.143, 6, 6 },
};

It’s possible and valid to mix and match these rules, so drips can operate in a combination ‎of fixed colors, random selections, or groups of each. It’s all in how those last two numbers ‎are set.‎

Icicle Effect

The upper “dribbling” section of each strip can be partially lit to give a sort of icicle effect, ‎with each drop pausing there before dropping. This can be seen in the Holiday Icicle Lights ‎with Flair guide (but looks great with icky ectoplasm too!)‎

led_pixels_Back-Window-Anim-Smaller

Near the top of the code, look for:‎

Download File

Copy Code
#define ICE_BRIGHTNESS 0 // Icycle effect Brightness (0 to <100%)

Bump that number up a little…10 to 25 works well, probably don’t want more than that.‎

This effect does not pair well with the color randomization explained earlier (but is fine ‎with multiple fixed-color drips). The code works, it just looks bad when the icicles switch ‎hue.‎

Carrie Mode

Firepixie was incorporating this code into a gorgeous LED-festooned dress and had ‎a twisted idea: could there be a switch to turn the normally beautiful lights into blood? This ‎required only minimal changes, so yes, it’s in there, but disabled by default.‎

This requires adding either a SPST toggle switch or a momentary pushbutton (held down for ‎as long as the effect is active) connected between ground and any unused I/O pin, or ‎between two I/O pins.‎

To use this effect, add one extra color at the end of the palette[] array. For example, one ‎might have three pretty winter colors, and then suddenly, BLOOD:‎

Download File

Copy Code
uint8_t palette[][3] = {
  {   0,   0, 255 }, // Color 0 = Blue
  { 127, 255, 255 }, // Color 1 = Teal
  { 255, 255, 255 }, // Color 2 = White
  { 255,   0,   0 }, // Color 3 = Red
};

The drips only reference the first three colors (0–2). The fourth color (#3) is not mentioned in ‎the drip[] table. It’s a secret extra thing.‎

Download File

Copy Code
} drip[] = {
  { 16,  7, 0.157, 0, 2 }, // Randomly pick from palette 0-2
  { 19,  6, 0.174, 0, 2 },
  { 18,  5, 0.195, 0, 2 },
  { 17,  6, 0.16 , 0, 2 },
  { 16,  1, 0.21 , 0, 2 },
  { 16,  1, 0.21 , 0, 2 },
  { 21, 10, 0.143, 0, 2 },
};

There are two lines in the code, both commented out by default, which enable this feature. ‎Remember that you must have a switch or button to use this.‎

Download File

Copy Code
//#define CARRIE_PIN    A2
//#define CARRIE_GROUND A3

‎Un-comment the first line, change the pin number if you like, and then connect a switch or ‎button between this pin and any ground pin:‎

Download File

Copy Code
#define CARRIE_PIN    A2

Sometimes a project is already using every ground pin on the board. That’s okay…if another ‎GPIO pin is available, you can use this as a makeshift ground for the other side of your ‎switch or button to connect to:‎

Download File

Copy Code
#define CARRIE_GROUND A3

This second pin, if enabled, is strictly a signal ground. It’s working off a GPIO pin and ‎should not be used for carrying any substantial load like additional NeoPixels.‎

Enabling Carrie mode is not an instantaneous poof switchover. Each drip currently in ‎motion will continue in its current color and only switches over at the start of its next ‎‎“ooze.” This gives a nice effect as the NeoPixel strips gradually change over one by one. As ‎with the random color option, this doesn’t pair well with the icicle effect; probably want one ‎or the other.‎

Extra Drips

As explained on the Planning page, there are a couple of easy options if you want more than ‎seven drips…‎

  • You can drive 8 drips from one board, but you won’t get ground splats in that case.‎

  • You can just build multiple units. There’s nothing that needs to be synchronized ‎between them.‎

A third option is to split some of the output signals to multiple strips. This is a thing you ‎can do with NeoPixels…feed the same data output to two or more strips and they’ll all show ‎the same thing. I used this on the dragon to provide nine drips total…the first two drips, plus ‎the splats, are “recycled.”‎

drips_32

There are some gotchas doing it this way…‎

These drips are an exact copy. The ooze, dribble, drip, and splat all occur in perfect sync, so ‎it really only makes sense visually if there are two points at similar heights on your prop.‎

You’ll want to put some distance between them, or on opposite sides of the prop. This ‎makes the duplicate drips less obvious.‎

This is why I only added two extra drips on the dragon…there weren’t many positions where ‎the dribble would look right on another part of the skull, and I didn’t want an exact left/right ‎copy of everything.‎

If you add duplicates this way, start from NeoPXL8 output #0 and work up from there. ‎That’s so the duplicate splats sync up. Looking at the diagram above, you can see only two ‎splat pixels are needed on the extra strand, corresponding to the two extra drips. You don’t ‎want or need an entire duplicate splat strand.

MCX JACK TO BNC RF CABLE ADAPTER
מק"ט יצרן # 1531
MCX JACK TO BNC RF CABLE ADAPTER
Adafruit Industries LLC
מק"ט יצרן # 3249
EVAL BOARD FOR ATSAMD21
Adafruit Industries LLC
מק"ט יצרן # 4368
ADDRESS LED STRIP SPI RGB
Adafruit Industries LLC
מק"ט יצרן # 1612
ADDRESS LED MOD SERIAL RGB 1=5
Adafruit Industries LLC
מק"ט יצרן # 3857
FEATHER M4 EXPRESS ATSAMD51J19
Adafruit Industries LLC
מק"ט יצרן # 4537
NEOPXL8 FOR FEATHER M4 - 8 X DMA
Adafruit Industries LLC
מק"ט יצרן # 3975
NEOPXL8 FRIEND - 8 X STRANDS NEO
Adafruit Industries LLC
מק"ט יצרן # 4884
ADAFRUIT FEATHER RP2040
Adafruit Industries LLC
מק"ט יצרן # 2886
FEATHER HEADER KIT FML
Adafruit Industries LLC
TACTILE ON/OFF SWITCH WITH LEADS
מק"ט יצרן # 1092
TACTILE ON/OFF SWITCH WITH LEADS
Adafruit Industries LLC
מק"ט יצרן # 1260
FLORA PLATFORM RGB NEOPXL V2 4PK
Adafruit Industries LLC
מק"ט יצרן # 1312
ADDRESS LED MODULE SERIAL RGB
Adafruit Industries LLC
מק"ט יצרן # 3631
ADDRESS LED STRIP R/G/B/W
Adafruit Industries LLC
מק"ט יצרן # 1609
BREADBOARD GENERAL PURPOSE PTH
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.