Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
AS8510-Slide11

In summary, the AS8510 is a very flexible device especially designed for battery sensor applications including two independent acquisition channels. It has a wide range of sample rates as well as wide configuration possibilities. The device is tailored to accurately measure battery current, from mA range up to kA range in combination with a 100µΩ shunt resistor connected in series with the battery rail. The battery is becoming a major power source for many systems, replacing the engine in important systems previously powered by the engine.

PTM פורסם ב: