Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide13
Power handling in resistors depends on the overall appearance of the component. The flange has to be flat with no scratches, otherwise air pockets with very high thermal resistance will form. This could lead to failures in the field due to hot spots. Bourns uses high quality copper in its flanges for this reason. The thickness of the flange leads itself to less pliability and better coplanarity, so Bourns offers a unique 6 mm flange thickness.
PTM פורסם ב: