Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide15
Open air shunts are used within the current measurement section of a power electronics application such as three phase motor windings or a domestic meter. This shunt should have very low resistance, low TCR, high current capability, and be cost-efficient. The PWR4412 has very good surge capabilities as well as a TCR of 20 PPM which is as good as the preferred material for shunts, manganin.
PTM פורסם ב: