Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide18
Most inverters could be expected to operate at temperatures as high as 85°C. The CRA2512 is rated to 3W but should already be derated at 85°C. Running 1W through the device at 85°C, the temperature on the chip is about 100°C which is quite acceptable.
PTM פורסם ב: