Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide14
Shown here is a retrofit example of how the XP Gen 2 provides multiple design possibilities for existing XP Designs. In this example, the designer replaced 7 XP-Gs with 7 XP-G2s and the result is over 30% better lumen output and over 30% light output using the same number of LEDs at a comparable cost. The designer also looked at a lower cost solution with comparable performance to the original with the XP-E2 LED. In this example, 7 XP-Gs were replaced with 7 XP-E2s and, as one can see from the table, the designer was able to get similar if not better performance than the original design, again at a significantly lower cost.
PTM פורסם ב: