Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide15

The same kind of increase in performance can be realized in flashlight designs as well. As the chart shown here, shows by simply dropping in an XP-G2 to an existing XP-G based flashlight one can achieve 20% more lumens and 20% better peak intensity while maintaining the same beam appearance. In the image, the designer has put together the beam from the XP-G and the XP-G2 side by side for better comparison. The beam on the left is the XP-G and on the right is the XP-G2, notice how much brighter the XP-G2 is.

PTM פורסם ב: