Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Single-Mode Bluetooth Smart System-on-Chip Solution Slide 16

If stand alone operation is required without the support of an external upgradable program memory the internal programmable ROM can be used. Software development can be on device RAM based with OTP only being needed at mass production stage.

PTM פורסם ב: