Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Single-Mode Bluetooth Smart System-on-Chip Solution Slide 8

The ARM Cortex M0 provides a lower µW for MIPS of any competitive µCore. This and the ability to use a single alkaline cell for power allows the lower power operation. The RF operation is not compromised by this low power operation with the DA14580 providing one of the best in class performances.

PTM פורסם ב: