Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List Associated Content
thermal2

Packages with exposed thermal pads are needed for higher power dissipation. The thermal resistance of the TO220 package can be as low as 2.7°C per watt. It now becomes a matter of designing the proper pad size or using thermal vias to provide a path for the removal of the heat.

PTM פורסם ב: