Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List Associated Content
summary

In summary, an LDO is a simple device that provides an accurately regulated output voltage protecting sensitive components. The input/output capacitors are the commonly used components for LDOs. The values of both capacitance and ESR vary with temperature. Verifying that the selected capacitor will remain within these needed specifications over the entire temperature range of the application is essential.

PTM פורסם ב: