Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
mesh tree route
Tree links, or direct associations, are shown on this slide with solid lines. Mesh links are indicated on the diagram by the dotted lines. A message may take multiple paths, particularly if one path is inaccessible, to ensure that the data reaches the appropriate node with or without passing through the coordinator. In tree routing, the message path follows the direct lines of association, child to parent/parent to child, as shown by the grey arrows. In mesh routing, there are more options along the mesh links and a more direct route can be followed.
PTM פורסם ב: