Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
thermoplastics
Unlike rubber thermoset elastomers which can be permanently hardened by heat, thermoplastic insulation will soften and become formable when heat is applied. After being heat extruded (molded), the thermoplastic insulated conductor must pass through a water trough to produce a hard finish to the material. The thermoplastic insulation will soften again if exposed to excessive heat or open flame. If enough heat is applied, the material will become so soft it will flow like melted candle wax.
PTM פורסם ב: