Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
braided shields
Braided shields are woven the same way as textile braids; however, instead of using yarn, copper strands or aluminum strands are used to make the braid. Braided Shielding removes 80-90% of externally generated noise. Braiding also provides longitudinal strength and is used when constant flexing is required, such as microphone cables.
PTM פורסם ב: