Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
coaxial
Coaxial cables have two cylindrical conductors with a common axis that are separated by a dielectric. A dielectric is a material or medium between two conductors which can sustain an electrical field and does not conduct electricity. The most common example of a dielectric is air and the most common example of a dielectric material used in coaxial cable is polyethylene. The braid shield is used as a signal return. Coaxial cables are used for radio frequency signal transmission and video applications including HDTV and cable TV.
PTM פורסם ב: