Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Linear-Slide11

Honeywell’s Linear Hall-Effect Sensor ICs may be used for basic current sensing for motor load monitoring and detection. They can also be used in appliances to monitor the current powering the electromagnets in the appliance’s motor. If the current is not within its normal range, the logic could also perform overload or motor malfunction detection.

PTM פורסם ב: