Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Linear-Slide9

A water pump is essentially a special application of an electric motor. These pumps are commonly manufactured for home appliances. Honeywell’s Linear Hall-Effect Sensor ICs may be used to generate an enhanced control signal for better resolution of the rotor position, which can improve the motor's efficiency. A crude RPM measurement would verify that the pump is working properly. The output of the sensor may be used as an alarm or a shut-off signal to help prevent motor overload.

PTM פורסם ב: