Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Supercap-Slide4

This slide assists users in selecting the series for a certain application. The horizontal axis represents backup time, or the amount of time the energy is needed. The vertical axis is ESR, going from high at the bottom to low ESR at the top. A real time clock application, for example, is one that requires a longer backup time, while an LED camera phone flash requires low ESR. Inside the triangles are the product families which meet the different requirements.

PTM פורסם ב: