Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Supercap-Slide6

This presentation will now explore specific applications and markets for supercapacitors. On this slide, there is a schematic of a power source that is providing power to an LED. For this example, the power source is a solar panel. When the sun is out the sun shines on solar panel, which is represented here as the “power source”. This charges up the supercapacitor and powers the LEDs. When it’s dark, the supercapacitor becomes the sole power source for the LEDs.

PTM פורסם ב: