Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
CAS-Slide17

It is possible to overdrive the internal reference of the CASR and CKSR models. This will change the zero-current output voltage. When raising or lowering the reference voltage, keep in mind 3 points: First, the output of the transducer will always be limited with a minimum of 0.375V and a maximum of 4.625V. Second, the measuring range will be determined by the maximum compensation current which is determined by the internal workings of the ASIC. A LEM applications engineer can help the designer determine what the maximum measuring range would be for a specific reference voltage. Third, the current source/sink of the Vref pin is based on its internal resistance, 680 Ω.

PTM פורסם ב: