Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
HO8-Slide10

Shown in the tables on this slide is the full range of the HO series programmable features. For instance Vref voltage can be programmed from 0.5V to 2.5V and the overcurrent detection can be set in the range of 0.6x to 5.8x the nominal rated current. There is a relationship between response time, bandwidth, and noise filtering that must be kept in mind during programming.

PTM פורסם ב: