Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
MCU-Slide14

The first member of the dsPIC family that will be covered in this presentation is the dsPIC30F. As indicated by the red blocks, the 16-bit core now has the addition of a DSP engine. The DSP engine can perform 16 x 16 multiply and accumulate operations in a single cycle. The accumulator is 40-bits wide to allow for overflow from multiply operations which would normally provide a 32-bit result. A CODEC interface is available for speech purposes. One of the primary applications for the dsPIC family is in motor control. This is made possible by a special motor control PWM peripheral along with a quadrature decoder interface, which helps locate the position of a rotor in a motor control. Some products also offer high speed Switch Mode Power Supply (SMPS) PWMs.

PTM פורסם ב: