Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
PIC18-Slide19

A number of application examples are provided with the PIC18FXXK20 Demonstration Board. One of these applications uses a Discrete Fourier Transform (DFT) to highlight the performance characteristics of the new PIC18FXXK20 MCU. As shown in the figure, this application uses a microphone connected to the audio input on the demonstration board. This signal then passes through a Low-Pass filter to the 10-bit ADC. The digitized samples are then transformed to the frequency domain using a DFT and displayed as a 16-point spectral representation on the board’s display.

PTM פורסם ב: