Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 10
In the microcontroller’s Deep Sleep mode, several processes can remain operating. The RTCC can be configured to keep time during Deep Sleep. It can even continue to output a seconds clock signal. Other I/O pins will maintain their state during Deep Sleep and throughout wake-up until the Deep Sleep “RELEASE” bit is cleared. Deep Sleep registers will retain data over Deep Sleep, even though the rest of SRAM is powered-off. If more data is needed, an application can use the table read/write features to save data to FLASH memory. On some devices, EEPROM memory is also an option. The DSBOR feature can be enabled to provide an indication of integrity for the special Deep Sleep and RTCC registers in case power levels dropped too low for safe operation. In addition to these features, several different wake-up sources can be enabled to operate through Deep Sleep.
PTM פורסם ב: