Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 5
Deep Sleep reduces current to minimum levels by turning off power to most of the chip’s SRAM, and cutting current consumption to 90% less than traditional Sleep mode. While most SRAM does not retain its data when powered-down, there are two general purpose Deep Sleep registers that will remain powered, allowing some context data to be retained. If more data needs to be saved, self-programmed FLASH (or EEPROM memory, if available) is an option. On parts with an internal core voltage regulator, the regulator is shut down during Deep Sleep to conserve power. The voltage regulator needs time to stabilize before the part can wake up from Deep Sleep, therefore Deep Sleep can typically take 1 to 2 milliseconds to exit on these parts. On devices that do not have a core voltage regulator, wake-up times will be much faster, typically 50 µs. Waking up from Deep Sleep causes a Power-On Reset, so execution will resume at the Reset vector rather than at the instructions that follow the sleep instruction. Special Function Registers will reset to their Power-On Reset default values. However, certain registers (such as TRIS) will not affect device behavior until the Deep Sleep “RELEASE” bit is cleared later by software. The RELEASE feature will be discussed later during the firmware overview.
PTM פורסם ב: