Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 14
The RTCC can keep a running clock of the current date and time, it also has an alarm feature that can be used to wake the microcontroller from Deep Sleep at a specified date/time. Unlike the DSWT, granularity is not restricted to 16 options; any date/time can be used. The internal low-power RC oscillator or the secondary oscillator can be used for a clock source, just like the DSWT. If both the RTCC and DSWT are going to be used, and robustness is not a key concern, the same clock source can be used so that power isn’t wasted keeping two oscillator circuits running. During Deep Sleep, I/O pins are generally held constant in their last configured state. However, the RTCC can be configured to output an alarm pulse or seconds clock output on the RTCC pin, even while the microcontroller is in Deep Sleep. This pulse could be used to continuously blink an indicator on a clock read out, for example.
PTM פורסם ב: